Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 35

Shown here is an example of how the screen looks when the customer uses the PractiSPIN for a stepper motor. The user can set the stepping mode normal, half-step, micro-step, can select the device, can select the decay mode slow or fast, the direction forward or reverse, the acceleration rate, the running speed, and the deceleration. So it really gives the customer a lot of flexibility and it is very easy to use.

PTM פורסם ב: