Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 21

Finally, the L6208 and L6228 devices have a full stepper driver with an embedded stepping sequence generator. This device is dedicated and optimized for stepper motors. A very simple microcontroller can drive the motor by simply selecting the kind of control, slow or fast decay, or a mix of the two. The microcontroller can select the kind of stepping sequence, half, full or micro stepping, and feed the step clock and the desired direction. The device does the rest, it is constantly moving. The PWM modulator described for the L6207 is also present.

PTM פורסם ב: