Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 11

The DC motor architecture can be controlled with the same product family presented in the previous slide. Because most of these products are dual bridge drivers, they can drive two DC motors or they can be used with outputs connected in parallel to drive a single DC motor. Every time the outputs are connect in parallel, the system dissipation is significantly reduced, because the Rds(on) is reduced.

PTM פורסם ב: