Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 16

Shown here is the simplified block diagram of a non-dissipative over current protection. No external sensing resistors are needed. This gives high accuracy and a non-dissipative solution with a cost-saving BOM. The working principle is very simple: the current of the power stage, sourced to the windings of the motor, is internally mirrored and compared with a reference current. Once the threshold current is reached, the driver is switched off for a time, fixed by the voltage charging time of the external capacitor connected to the enable pin.

PTM פורסם ב: