Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
powerSPIN Motor Control ICs Slide 10

The two-phase bipolar stepper motor architecture includes the controller, the driver and the power stage are embedded in part of ST’s monolithic family, whose part numbers are highlighted in yellow shown here. Some of the other monolithic devices, highlighted in grey, are integrating the power stage only, with a variable set of embedded protection and diagnostic features, can be used to drive Stepper motors driven by an external controller.

PTM פורסם ב: