Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
STM32 Connectivity Line Slide 18

Shifting focus to the software solutions available for the STM32 connectivity line, ST supports the STM32 with a free software library including program examples. The libraries and examples are written in ANSI-C and provide high-level functions for configuring and using all the available peripherals. These libraries are compliant with the CMSIS standard, which is a vendor-independent hardware abstraction layer for the Cortex processor to simplify software reuse across different platforms. ST also offers a free motor control library supporting sensorless vector control for 3-phase brushless motors. A free DSP library covering PID, IIR, FFT, and FIR is also available. Finally, a free USB device library is available and supports the following USB classes: mass storage, HID, DFU, CDC and audio.

PTM פורסם ב: