Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
STM32 Connectivity Line Slide 25

The USB Host and OTG demos are based on micro-C/OS-2 RTOS and micro-C/USB stack from Micrium. HID, mass storage and OTG dual role device examples are available. The software is delivered in binary format and the USB device demos are based on the ST free software library. USB mass storage, HID such as mouse and keyboard, and CDC device demos are also available in source code.

PTM פורסם ב: