Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 11

Looking at the wave forms shown on this slide, the top trace is aliased, the frequency is reading 9.91 MHz. On the bottom trace, with a different capture, the frequency reads 491.1 MHz, which is the proper frequency of the capture. Therefore, even though the wave form looks proper, the upper wave form is aliased due to sampling at a much lower frequency than the real frequency of interest.

PTM פורסם ב: