Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 4

When looking at oscilloscopes there are two types of bandwidth. There is the analog bandwidth, which is essentially the bandwidth of the amplifier on the front end. Typical instruments have a classification of 100 MHz, 500 MHz, 1 GHz and so on. There is another item called digital bandwidth, which is dependent on the sample rate and therefore is also dependent on the acquisition memory size which can affect the sampling rate.

PTM פורסם ב: