Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 50

The oscilloscope screen shot on this slide shows the effect of the inductance of the probe ground lead. As the ground lead length increases its inductance also increases, causing an ever increasing amount of distortion. The waveform on the extreme left, the olive green trace, is measured with a standard length ground lead. It has the highest amount of overshoot, approximately 36.6%. The second capture, brown, used a high frequency compensated ground lead and the overshoot was reduced to 26.6%. The third trace, blue, illustrates the use of a ground spring, which is really short. This reduced the overshoot to 17.6%. The final two, light green and red, are the best, using the ground blade and a probe head ground achieved an overshoot of 16.3% and 10.1% respectively. The 10.1% overshoot is very close to being an accurate representation shape of the actual signal overshoot. This is a good example of why it is important to keep the grounds as short as possible to transfer the true wave form into the oscilloscope.

PTM פורסם ב: