Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List

Sampling Interleaved Sampling

Random Interleaved Sampling, RIS, (also often called "equivalent time mode") is an acquisition technique that allows effective sampling rates higher than the maximum single-shot sampling rate. It is used only on repetitive waveforms with a stable trigger. The RIS sampling is achieved by making multiple single-shot acquisitions (shown in this slide as successive acquisitions in different colors) at the maximum real-time sample rate. The instrument then interleaves these acquisitions to provide a waveform that is a multiple of the maximum single-shot sampling rate - maybe even 100 times faster sampling. However, it will take the instrument a longer time to generate a RIS waveform since it must collect the waveform data of multiple acquisitions. This will depend on the trigger rate.

PTM פורסם ב: