Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 41

To this point the presentation has discussed the basics of an oscilloscope. It will now focus on how to get the signal of interest to the oscilloscope. The discussion will be about different probing techniques, including passive probes, which are typically standard with most modern oscilloscopes. Passive probes vary in bandwidth from 350-500 MHz and in some of the lower end products 100 MHz passive probes are available. Active probes will also be discussed in depth. These are typically higher in bandwidth, much greater than 500 MHz and require power because they are transistor based. There are also differential probes which require the user to use one channel as opposed to using two single ended probes and then doing the math, subtracting one from the other. High voltage probes are useful when debugging and troubleshooting high voltage power supplies, for example. Finally, there is a wide variety of current probes for measuring current.

PTM פורסם ב: