Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 51

In summary, the heart of an oscilloscope is the acquisition system. Analog bandwidth is the bandwidth of the amplifier at the front end, digital bandwidth is dependent on the sample rate and acquisition memory size which can affect the sampling rate. Real time sampling is good for capturing transient signals and is the default mode in most oscilloscopes. Random interleave sampling, or equivalent time sampling is only usable for repetitive signals not transients, but gives a higher effective sample rate. Roll mode is a good selection for very low frequency signals. There are many modes to start the scope such as auto trigger, single shot trigger, trigger on any of the four inputs, or an external trigger. Cursor measurements are easy to set up and are based on display resolution and the accuracy of the user placing the cursor properly. Parameter measurements offer higher accuracy, and do not rely on display resolution, or the user placing the cursor. Parameters enable the use of full internal resolution of the instrument, and the ability to display histograms or statistics on the display. Modern oscilloscopes have math capabilities including add, subtract, multiply, and etc. Fast Fourier transforms are also common. Passive probes vary in bandwidth from 100-500 MHz. Active probes are typically higher in bandwidth, much greater than 500 MHz, but require power because they are transistor based. Differential probes allow the use of one channel rather than using two single ended probes and then having to do the math, subtracting one from the other. As the name implies, high voltage probes are useful when debugging and troubleshooting high voltage power supplies. Finally, current probes are available for measuring current.

PTM פורסם ב: