Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 13

Shown in this slide are some of the wireless options available, arranged in three approaches. This table shows the system architectures or system partitioning approaches that customers may want to consider. For instance, there may be a customer who wants a self-contained system on a chip. This customermay want to consider one of the CC devices, one of which is the CC430. Or the customer might want to look at an application MCU with an RF radio, with all of the wireless stacks residing on the microcontroller, such as an MSP430, along with the application. A third approach would be an application microcontroller where the MSP430 has the application, or a protocol processor such as the CC430 with the wireless stacks, along with the integrated transceiver.

PTM פורסם ב: