Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 25

In this slide, an example is shown of an MSP430 being used in an ECG application; specifically this is using the MSP430FG439, one of TI’s SoC devices. The application note, SLAA280A, provides all the technical details for this application. Basically there are electrodes providing an input into the microcontroller which performs signal conditioning, and then is capable of providing a heart rate output to the LCD. In addition, if the user has connected a serial cable to their computer, it is possible to view the ECG waveform. This is a simple example, but very applicable for the consumer and portable medical market. Also available online are the reference design, the software, and PC GUI.

PTM פורסם ב: