Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 27

The second application to be discussed is a pulse oximeter. The pulse oximeter measures the amount of oxygen in the blood and extracts the heart rate. It is used to determine how well oxygen is saturated in the blood. Typically the desired result is 100% oxygen saturation for a healthy person, or in the high 90% range. If the percentage is much lower than that, it is an indication of a possible problem in getting oxygen into the blood cells and spread properly throughout the body.

PTM פורסם ב: