Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 8

In the large gray bubble toward the top of the slide are technologies that are being developed or that have recently been introduced to the market. In the 5xx-6xx new generation family, are the F541x and the F543x; basically everything else in this large gray bubble is based on this new architecture. This includes the USB devices now on the market, which are the F550x, F551x, and F552x families. Another group of devices is our native sub-1V family that operates down to 0.9V without a regulator. And our FRAM-memory based devices with unique benefits such as fast write times and lower power consumption are already sampling. TI is also involved with integrating RF functionality, such as the CC430 devices. Finally, also in development are MSP430 devices that will feature more memory and capability, enabling higher functionality such as hosting connectivity stacks or RTOS capabilities.

PTM פורסם ב: