Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 9

Shown on this slide is a review of the SoC device features. The F563x and the F663x are higher memory devices with up to 256 kB of flash and 16 kB of RAM, and an additional 2 kB available if the USB controller is disabled. In addition, an A/D converter, a D/A converter, as well as comparators and other features will also be incorporated as needed; such as the RTC battery backup feature which allows the consumer to swap out a system battery without losing the RTC.

PTM פורסם ב: