Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 30

Shown in this slide is a generic portable medical application. There are many applications that are possible with the MSP430, such as blood glucose meters, pulse oximeters, digital thermometers, and more. There are a few basic blocks to which the sensors on the front-end can be added. The inputs from these will be amplified, filtered, and digitized to go into the microcontroller. The microcontroller will do the processing, and then display the result to the user. The benefit of the integrated LCD controller is evident in this application. The slide shows an FG479, which is capable of communicating via one of TI’s wireless transceivers, it is also capable of communicating over USB. Other capabilities such as voice, battery operation are also shown. In short, with a minimal number of external components, there are many possible applications with an MSP430 SoC.

PTM פורסם ב: