Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 22

As previously mentioned, Wi-Fi operates on the 2.4 GHz and 5 GHz bands. The 2.4 GHz band is an unlicensed frequency range with 3 non-overlapping channels allocated for industrial, scientific, and medical applications. Although in practice, the band can be used by products falling outside of these three categories such as consumer electronics. Products based on 802.11 b, g, or n operate on this band. It can be considered the default band for consumer applications such as microwaves, baby monitors, cordless phones, and many other devices that can be found in a typical home. With all these devices operating on the same band, it can get quite crowded and interference can be a problem as devices compete for space.

PTM פורסם ב: