Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 28

This page shows what a Wi-Fi system looks like from a hardware and software perspective. On the right side in red is a Wi-Fi (and in this case Bluetooth as well) transceiver device, for example the TI WL1271. The larger light gray box represents a Wi-Fi module, which may include additional RF components like a front end module, filter, clock, and antenna connecter. The transceiver will pair up with a host controller via an SDIO connection for Wi-Fi. The reason a microprocessor is required, is shown on the software portion of the diagram. A number of software components are required in a wireless system and thus require a processor to run them. The software includes an operating system, hardware drivers, stacks, profiles, and applications. The Wi-Fi device itself will also host some software, but typically only the firmware and MAC/PHY software.

PTM פורסם ב: