Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 21

WiFi Direct is a new standard which is making its way into new products, likely to be released at the end of 2011. Unlike the WLAN infrastructure mode network, WiFi Direct will allow devices to connect directly to each other rather than going through an access point. This will save time transferring data and create greater ease of communication. One device can serve as a group owner and allow multiple devices to connect to it. Wi-Fi Direct devices will also be WPA2 and WPS certified. There is also an existing feature called “Ad Hoc mode” which was originally intended to provide this same peer-to-peer connectivity. However, the implementation of Ad Hoc mode was extremely complex for the user and it was practically never used in the market. Wi-Fi Direct fixes the issues of Ad Hoc mode to allow true peer-to-peer networking.

PTM פורסם ב: