Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 8

The first step in getting a device Wi-Fi certified is to become a member of the Wi-Fi Alliance and get the product tested. If the device passes the certification test, it will be allowed to use the Wi-Fi logo. It is also important to note that chips or modules along with software can be pre-certified however the end product that uses them still needs to be certified. Finally, Wi-Fi certified products are also backwards compatible with previous generations, for example any product today can still work with older 802.11b solutions.

PTM פורסם ב: