Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 2

When and why does it make sense to use Wi-Fi? First and foremost, Wi-Fi allows devices to connect to each other, to the Internet, and to wired networks, all in a fast and secure way. It is the most widely used method of connecting computers to the Internet. Wi-Fi can be thought of as a wireless Ethernet because it provides performance that is similar to a wired connection like Ethernet. A key value of Wi-Fi is the high data rates that can be achieved, around 72 Mbps raw. Do to its advantages, Wi-Fi has become increasingly popular and widespread with over 2.5 billion units in the market and a projected 1 billion units to be release in 2011 alone.

PTM פורסם ב: