Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Introduction to Wi-Fi Technology Slide 3

To provide a better perspective of Wi-Fi, this page shows how it compares to other wireless technologies. The graph on the left, shows the range of each technology. Wi-Fi has a typical range of 100 meters which in a real-world situation equals about the range of a house. Also shown, are low energy technologies like Bluetooth and ANT which have a range closer to 10 meters or about the range of a large room. However, a big factor in range is whether a power amplifier is used with the radio. Regarding data rate or maximum throughput, Wi-Fi has the greatest throughput with up to 72 Mbps for 802.11n. Compared to other technologies, Wi-Fi has a higher power consumption but this is because it offers the highest data rates. Typically, portable Wi-Fi devices run on a lithium ion battery. However, depending on the data rates and how often data is sent, its also possible to use lower power sources such as AAA batteries.

PTM פורסם ב: