Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide16

The purpose of equalization is to compensate for the affect of a transmission line, specifically in a loss of signal strength. There are two areas where this loss can be compensated; at the transmit side using pre-emphasis as shown in the image on the top left of this slide, where voltage levels are emphasized by the same loss expected from the transmission line, and at the receiver edge where equalization is used to clean the distortion of the signal eye. The specific settings available on the Cyclone® IV GX are shown in the table.

PTM פורסם ב: