Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide6

Each receiver channel can be clocked by one of the two dedicated MPLLs associated with that quad. The CDR in each channel allows each receiver to align exactly to the data on that channel which minimizes or eliminates the affect of skew on bonded channels. Each MPLL provides two dedicated outputs to the transceivers, the CLK and CLK2x are additional outputs that can be used to feed the FPGA fabric. It is important to note that the MPLLs can only clock contiguous channels. Therefore, MPLL2 can drive channels two and three while MPLL1 drives channels zero and one, or MPLL2 can drive channels zero and one while MPLL1 drives channels two and three, but MPLL2 cannot drive channels three and one while MPLL1 drives channels two and zero.

PTM פורסם ב: