Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide23

In the case of Cyclone® IV E, the mathematics are straightforward. The core voltage of the Cyclone® IV E is lower than the 1.2V of the Cyclone® III. As such, the lower core voltage results in both static power and dynamic power savings resulting in up to 25% lower total power. In the case of Cyclone® IV GX, the comparison is made to a comparable system. In the current generation of products, external SERDES ASSPs are used for the high speed serial I/O interface to the FPGA. With Cyclone® IV GX integrated transceivers, the total power consumption to perform the identical function is 30% lower. By creating various test cases using industry standard SERDES components, and performing power comparisons, the data in the table on this slide shows that the most conservative system benefits with a 30% power savings. For larger designs and higher transceiver counts, the power savings can be greater.

PTM פורסם ב: