Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide2

Shown on this slide is a block diagram of the Cyclone® IV GX device showing the relational placement of the major blocks. The specific innovations for the Cyclone® IV GX are the integrated transceivers that address most mainstream 3G applications, the integrated PCIe hard IP that supports x1, x2 and x4 lanes along with rootport and endpoint configurations, and the MPLLs and the resulting changes to the clock networks throughout the FPGA.

PTM פורסם ב: