Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide24

Not only is the power consumption of the Cyclone® IV family setting a standard, but the power supply network requirements of the Cyclone® IV are also innovative. Through the use of internal regulators and careful design, keeping the customer’s total cost in mind, the Cyclone® IV E and GX devices both only require two power voltage rails and two regulators to supply the required VCCINT and VCCAUX rails. Keep in mind that any I/O standard required that does not use 1.2V or 2.5V (or in the case of Cyclone® IV E, 1.0V for VCCINT), additional power supplies are required. Additionally, the Cyclone® IV devices do not require any specific power sequencing to operate, enabling them to be fully hot-swap capable.

PTM פורסם ב: