Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
MS-Slide13

The HMC1001 1-Axis and HMC1002 2-Axis sensor components provide the most resolution available at 27 µGauss. These sensors also include Honeywell's patented on-chip “Set/Reset” & “Offset” straps which are used to eliminate the effects of stray magnetic fields, temperature drift, amplifier offsets and drift. The HMC1001 and HMC1002 are the most sensitive magnetic sensors offered by Honeywell.

PTM פורסם ב: