Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 16
Simply put, the flash accelerator attempts to have the next Cortex-M3 instruction that will be needed in its latches in time to prevent CPU fetch stalls. Internally, the flash accelerator includes an array of eight 128b buffers to store both instructions and data in a configurable manner. The operations within this module are completely transparent to the end user. Programming this block is achieved by the “FLASHCFG” register alone. After reset, the flash accelerator defaults to the enabled state. Software can turn memory access acceleration on or off, or change the acceleration configuration at any time. Following reset, the flash access timing is also set to a default value of 6 CPU clocks. This is considered as a “safe setting” and will work for any condition. As an illustration, if the application needs to execute at 20MHz, the timing can be set to 1 CPU clock and if the application needs to execute at 100MHz, the timing can be set to 5 CPU clocks. Flash programming operations are not controlled by the flash accelerator, but are handled as a separate function.
PTM פורסם ב: