Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 2
The LPC1700 is pin-to-pin compatible with the popular ARM7-based NXP LPC2300 series, which allows for a smooth migration for ARM7 customers to move on to Cortex-M3. The NXP implementation of Cortex-M3 has the following key implementations: an MPU (Memory Protection Unit), which can be a great complement for an RTOS based application; a NVIC (Nested Vectored Interrupt Controller) that offers defined interrupt latency; and a WIC (Wakeup Interrupt controller) that allows fast wakeup from power down modes. The Flash Accelerator in the NXP Cortex-M3 allows the devices to execute out of Flash with zero-wait states. The LPC1700 also has excellent DMA support that fully enables the high end serial interfaces like USB, Ethernet and CAN. With 15 serial interfaces, this device is tailored for communication. The LPC1700 is more power efficient in active mode and it would consume less than 1uA in Deep Power down mode. Also, the LPC1700 is currently the industry’s fastest running Cortex-M3 processor at 100MHz.
PTM פורסם ב: