Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 9
To overcome this restriction, a technique called bit banding allows direct bit manipulation on sections of the peripheral and SRAM memory spaces, without the need for any special instructions. The bit addressable regions of the Cortex-M3 memory map are composed of: the bit-band region (which is up to 1MB of real memory or peripheral registers) and the bit-band alias region, which takes up to 32MB of the memory map. Bit-banding works by mapping each bit in the bit-band region to a word address in the Alias region. So by setting and clearing the aliased word, address bits can be set and cleared in the real memory. This image shows a bit-banding example for the SRAM region.
PTM פורסם ב: