Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 3
The table shows all the derivatives of the LPC1700 series and breaks them into 2 divisions based on their pin-counts, 100-pin and 80-pin. The Flash and RAM are available in several sizes as is shown here. Of the 100-pin package devices, the LPC1768 is the most featured in this series with the highest possible RAM and Flash configurations and a full peripheral set. The next set of devices is based around an 80-pin package which has Flash sizes from 32KB to all the way up to 512KB. The LPC1751 is the least featured device in this series with 32KB Flash, 8KB RAM and an equipped USB module.
PTM פורסם ב: