Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 48
This highlights the key features of the RTC block. The block measures the passage of time to maintain a calendar and clock; provides seconds, minutes, hours, day of month, month, year, day of week, and day of year; and has ultra-low power design to support battery powered systems. Less than 1µA is required for battery operation and uses power from the CPU power supply when it is present. The dedicated 32 KHz ultra low power oscillator also has a dedicated battery power supply pin that is isolated from the rest of the chip. The RTC will work down as low as 2.1V.
PTM פורסם ב: