Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 43
Complementing the motor control PWMs is the Quadrature Encoder Interface (QEI) block. The QEI module decodes the digital pulses from a quadrature encoder wheel to integrate position over time and determine direction of rotation. The digital pulses from an external quadrature encoder wheel can be decoded to integrate position over time and determine direction of rotation. By monitoring both the number of pulses and the relative phase of the two signals, the position, direction of rotation, and velocity can be tracked. The Index signal (3rd signal) can be used to reset the position counter. In addition, it can capture the velocity of the encoder wheel. The QEI tracks encoder position and increments/ decrements depending on direction with three position compare registers with interrupts and is programmable for 2X or 4X position counting. By using 32-bit registers for position and velocity, the QEI can be used for velocity capture using a built-in timer with a compare function and interrupt. The QEI first received three input signals: phase A (PHA), phase B (PHB), and index. By monitoring the phase of the first two signals, the QEI can detect if the encoder wheel is moving in a forward or backwards direction. The index signal provides the absolute position of the wheel.
PTM פורסם ב: