Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LinkSwitch-II Overview Slide 10

The LinkSwitch-II is available in the P package (DIP-8C), G package (SMD-8C), (LNK6x6 only), and D package (SO-8C). As shown in the figures, these packages use four source pins on one side for optimized thermal resistance and three pins on the opposite side to increase creepage distance and reliability.

PTM פורסם ב: