Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LinkSwitch-II Overview Slide 13

Next, the target oscillator frequency is set between 55 kHz and 85 kHz. The 85 kHz limit is selected 15% below the maximum frequency to allow frequency compensation for primary inductance variations. This limit does not apply to CV-only designs. The diode conduction time (DCON) value is also set between 4.5 µs to 8 µs.

PTM פורסם ב: