Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 14

This is a practical explanation of how this is done. Illustrated here is a controller with four sensors, or four copper pads, and each one of them is connected through four copper traces of different length. At the beginning, the intrinsic capacitance will be different because the channel with the sensor that is farther away will have a higher capacitance. As mentioned before, working with both external capacitors and the reference capacitance (which can be changed through a register), the user can equalize those capacitances to be as close to each other as possible and bring them within the actual dynamic range. By doing this, the objective of putting the system in a condition as balanced as possible is achieved, assuring that the controller will properly detect capacitance changes due to user touch.

PTM פורסם ב: