Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 5

Capacitive sensing technology is based on the detection of the capacitive effect of the human finger. Whenever there is an electrode and a finger is put on or close to it, capacitance is being added. Thus, the controller detects a capacitance change, and, depending on the settings of its registers, it identifies whether it is a touch or not. It is a very simple implementation as far as the sensor goes, because it is only a copper pad, and it can have different shapes, as can be seen on this slide.

PTM פורסם ב: