Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 29

Although the capacitive controllers available now have not been designed to work with capacitive LCD touch screens, it is possible to emulate that capability using a transparent resistive overlay on top of an LCD screen. There would have be a chequered pattern of sensing areas, a transparent overlay divided in squares or rectangles with the number of inputs matching those that the capacitive touch controllers support. Basically, the LCD display must be divided into discrete zones and then a graphic interface is designed with a virtual button on the screen. It is not a full capacitive touch implementation, but in cases where continuous tracking capability is not needed, it is a way in which this can be done. The transparent overlay used would be an ITO (Indium-Tin Oxide) on glass.

PTM פורסם ב: