Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 7

This illustration shows a simplified block schematic of STMicroelectronics’ capacitive sensing controllers. On the left, a host controller is required which communicates through I2C with the touch sensing controller. The copper sensing pads are shown on the right with the traces going into the front end of the detection engine. This is an example of a “Finite State Machine”. That means it has some intelligence built-in and registers they can access, but they are not micro-controllers. A couple of the advantages are that there are no worries about programming and memory or loading software. Communication is through I2C where the user can access the registers and transfer the data, or have available a “direct output” call on the GPIO mode, which means that some of the GPIOs can be activated directly without even going through the micro.

PTM פורסם ב: