Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 20

Other registers are those that allow the set up the filters. There are two kinds of filters. The primary filter operation is based on integration time and the strength threshold. The integration time filter sets the number of samples that are going to be collected before the controller decides whether there was a touch or not. The strength threshold sets the minimum number of readings that must exceed the reference plus the TVR to have a touch considered as such.

PTM פורסם ב: