Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 17

Guidelines are listed here for sensor routing, or how to bring the signal from the copper pad acting as the capacitance sensor to the input of the device. It is recommended, in general, to use a via to connect to the middle layer. Use short routing if possible and avoid having traces run parallel to each other to minimize capacitance. Any physical layout that may create unwanted capacitance should be avoided as much as possible. If that is not possible, then care should be taken to have a distance or a gap between them, as wide as possible. The empty spaces on top of wires should be filled with mesh ground as protection against noise, and the ground polygon clearance should be at least half a millimeter. It is always a good design practice to keep the sensor traces away from I2C lines or any other digital lines that might be sources of noise.

PTM פורסם ב: