Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 30

Touch Sense can be used also for industrial controls. One of the many advantages of touch sensing is that there are no moving parts and no holes through which dust or other agents can get in, making it very robust. In essence, there can be a completely flat panel made of glass or plastic material utilized as the user interface, resulting in a completely sealed front panel, impervious to most environmental conditions.

PTM פורסם ב: