Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
healthcare-wellness-slide23

The M24LR16E RF event pin replaces the E1 pin and can be programmed to toggle on an RF communication as a busy indication, or a write operation as a WIP indication. This enables the MCU to know when the RF host is communicating with the M24LR16E and if the content of the memory is being changed, without the need to poll for an I²C ACK.

PTM פורסם ב: