Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
healthcare-wellness-slide4

Costs to treat a growing population afflicted with obesity, chronic disease, and the elderly are growing at an alarming rate. Additionally, the difficulty of these patients in getting to the doctor’s office or clinic can be major to extreme. A solution may be to move patients out of the hospital to home, with remote monitoring of the patients. The benefit is that patients, particularly the elderly, tend to mend better in their homes, once the requirement for urgent critical or intensive care has passed. There is less chance of infection from secondary diseases due to extended stays in-hospital, and costs are reduced for both the patient and the insurance provider.

PTM פורסם ב: