Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 20

The Constant Current/Constant Voltage IC summary table on this slide shows the products that are offered in the TSM and SEA families. The package types can be seen, the IC current requirements for each, plus some of the older devices that had higher Icc currents, in the range of 1 mA, 0.7 mA, or 2 mA. This table illustrates how ST has reduced the Icc current consumption with the newer products. This in turn is helping reduce the no-load current consumption in the power supply.

PTM פורסם ב: