Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Secondary Side Switch-Mode Power Supply Control Slide 22

The product applications for synchronous rectification controllers include adapters, AC–DC power supplies including power supplies for servers, and a variety of DC/DC converters. Synchronous rectification is used to increase power supply efficiency by reducing the losses associated with output rectification. With SR the device that is being used for the output rectification is a MOSFET. Replacing a Schottky rectifier with a MOSFET results in lower power losses. The MOSFET is used with the SR controller commutating it on when the current would be flowing in the forward direction through the body diode, effectively synchronizing it with this event, hence the name. When the body diode would be reverse biased, the MOSFET is turned off and the reverse biased intrinsic body diode of the MOSFET then blocks reverse current flow. In the case of the non-synchronously rectified power supply, the power loss across the Schottky diode or rectifier is calculated by taking the voltage drop across it times the current (P loss =E (voltage) x I (current)). With the MOSFET, the voltage drop across it is the product of the current (I) times the on-resistance (Rdson), the power lost across it is the I-squared-R power loss of Rdson resistance of the MOSFET, or the MOSFET on-resistance times the current squared (P loss = I2 x R). The reason for using the MOSFET is that the channel on-resistance is quite low when it is fully saturated or fully turned on. This means it is going to provide a much lower power loss because the voltage dropped across the MOSFET will be lower than the forward voltage drop across a Schottky rectifier. That is why synchronous rectification is employed more and more in power supply designs, to significantly reduce the output rectification power losses and greatly improve the overall efficiency of the power supply. What ST has devised is a family of controllers that allow driving the MOSFETs the right way, so that they work as synchronous rectifiers.

PTM פורסם ב: